InterfaceObjectInvalidState Enumeration¶
NXOpen.Assemblies.ProductInterface.InterfaceObject.InvalidState is an alias for NXOpen.Assemblies.ProductInterface.InterfaceObjectInvalidState
-
class
NXOpen.Assemblies.ProductInterface.
InterfaceObjectInvalidState
¶ Bases:
object
Invalid state of problematic product interface object
Enum Members
Enum Member Enum Member Description Valid product interface has no issueSleeping product interface is sleepIncorrectOrphan product interface is in an incorrect orphan stateSelfReferenced product interface references itself-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-