Collection Class¶
-
class
NXOpen.Assemblies.ProductInterface.
Collection
¶ Bases:
object
This class represents the collection of product interface objects
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateObjectBuilder | Create Product Interface Object Builder @return |
CreatePropertyBuilder | Create Product Interface Property Builder @return |
FindObject | Find the Product Interface Object with input name @return Product Interface Object with this identifier |
GetProductInterfaces | Returns all the product interface objects in the part @return product interface objects in the part |
Method Detail¶
CreateObjectBuilder¶
-
Collection.
CreateObjectBuilder
¶ Create Product Interface Object Builder
Signature
CreateObjectBuilder()
Returns: Return type: NXOpen.Assemblies.ProductInterface.ObjectBuilder
New in version NX5.0.0.
License requirements: None.
CreatePropertyBuilder¶
-
Collection.
CreatePropertyBuilder
¶ Create Product Interface Property Builder
Signature
CreatePropertyBuilder()
Returns: Return type: NXOpen.Assemblies.ProductInterface.PropertyBuilder
New in version NX9.0.0.
License requirements: None.
FindObject¶
-
Collection.
FindObject
¶ Find the Product Interface Object with input name
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the product interface object you want Returns: Product Interface Object with this identifier Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
GetProductInterfaces¶
-
Collection.
GetProductInterfaces
¶ Returns all the product interface objects in the part
Signature
GetProductInterfaces()
Returns: product interface objects in the part Return type: list of NXOpen.Assemblies.ProductInterface.InterfaceObject
New in version NX10.0.2.
License requirements: None.