WeldStandard Enumeration

class NXOpen.Annotations.WeldStandard

Bases: object

Specifies the weld standard Enum Members

Enum Member Enum Member Description
Ansi
ANSI standard
Din
DIN standard
Jis
JIS standard
Iso
ISO standard
Eskd
ESKD standard
Gb
GB standard
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.