ToleranceZoneShape Enumeration

class NXOpen.Annotations.ToleranceZoneShape

Bases: object

Specifies the tolerance zone shape Enum Members

Enum Member Enum Member Description
Planar
Specifies planar zone shape
Cylindrical
Specifies cylindrical zone shape
Spherical
Specifies spherical zone shape
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.