TolerancePlacement Enumeration

class NXOpen.Annotations.TolerancePlacement

Bases: object

Specifies the tolerance text placement relative to the dimension text Enum Members

Enum Member Enum Member Description
Below
Specifies tolerance below dimension text
After
Specifies tolerance after dimension text
Above
Specifies tolerance above dimension text
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.