TextWithEditControlsBuilder Class

class NXOpen.Annotations.TextWithEditControlsBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Annotations.TextWithEditControlsBuilder which collects internationalized text strings from the user for processing on an annotation object.

This is a sub-builder class and cannot be directly instantiated

New in version NX6.0.0.

Properties

Property Description
Tag Returns the Tag for this object.
TextBlock Returns the text with symbols builder

Methods

Method Description
GetEditorText Text from the editor text @return
SetEditorText Text into the editor text
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

TextBlock

TextWithEditControlsBuilder.TextBlock

Returns the text with symbols builder

-------------------------------------

Getter Method

Signature TextBlock()

Returns:
Return type:NXOpen.Annotations.TextWithSymbolsBuilder

New in version NX6.0.0.

License requirements: None.

Method Detail

GetEditorText

TextWithEditControlsBuilder.GetEditorText

Text from the editor text

Signature GetEditorText()

Returns:
Return type:list of str

New in version NX6.0.0.

License requirements: None.

SetEditorText

TextWithEditControlsBuilder.SetEditorText

Text into the editor text

Signature SetEditorText(text)

Parameters:text (list of str) –

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)

Validate

TextWithEditControlsBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.