TextType Enumeration¶
-
class
NXOpen.Annotations.
TextType
¶ Bases:
object
Specifies the custom symbol text type Enum Members
- modified in the custom symbol. “
- “Arbitrary”, ” Specifies the default text defined in the master symbol
which can be modified in the custom symbol. The text can be single or multiple line text. “
“Controlled”, ” Specifies the text defined in the master symbol as enumerated- set of values, one of which can be selected in the custom symbol. “
- “PartiallyControlled”, ” Specifies the text defined in the master symbol as enumerated
set of values, one of which can be selected or overwritten in the custom symbol. “
“Integer”, ” Specifies ther text defined in the master symbol as an integerconstrained between maximum and minimum value. An integer value between minimum and maximum can be used in custom symbol. “
“Real”, ” Specifies ther text defined in the master symbol as an realconstrained between maximum and minimum value. An real value between minimum and maximum can be used in the custom symbol. “
“Last”, ” Last enum value. Should not be used. “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.