TargetPointBuilder Class¶
-
class
NXOpen.Annotations.
TargetPointBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.TargetPoint
builderTo create a new instance of this class, use
NXOpen.Annotations.TargetPointCollection.CreateTargetPointBuilder()
Default values.
Property Value Angle 0 Height 5 Width Thin New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns or sets the angle |
Color | Returns or sets the color |
Height | Returns or sets the height |
Inherit | Returns the inherit |
Location | Returns the location |
Tag | Returns the Tag for this object. |
Width | Returns or sets the width |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TargetPointBuilderThickness Enumeration | the types of target point thickness |
Property Detail¶
Angle¶
-
TargetPointBuilder.
Angle
¶ Returns or sets the angle
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Angle(angle)
Parameters: angle (float) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Color¶
-
TargetPointBuilder.
Color
¶ Returns or sets the color
-------------------------------------
Getter Method
Signature
Color()
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (Id) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Height¶
-
TargetPointBuilder.
Height
¶ Returns or sets the height
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Height(height)
Parameters: height (float) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Inherit¶
-
TargetPointBuilder.
Inherit
¶ Returns the inherit
-------------------------------------
Getter Method
Signature
Inherit()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Location¶
-
TargetPointBuilder.
Location
¶ Returns the location
-------------------------------------
Getter Method
Signature
Location()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Width¶
-
TargetPointBuilder.
Width
¶ Returns or sets the width
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Annotations.TargetPointBuilderThickness
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width ( NXOpen.Annotations.TargetPointBuilderThickness
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
TargetPointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.