TableSectionStyleBuilderContinuationPropertyType Enumeration

NXOpen.Annotations.TableSectionStyleBuilder.ContinuationPropertyType is an alias for NXOpen.Annotations.TableSectionStyleBuilderContinuationPropertyType

class NXOpen.Annotations.TableSectionStyleBuilderContinuationPropertyType

Bases: object

Represents the section continuation property

Enum Members

Enum Member Enum Member Description
Left
Left
Right
Right
Up
Up
Down
Down
NextSheet
Next Sheet
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.