TableSectionStyleBuilderAlignmentPositionType Enumeration

NXOpen.Annotations.TableSectionStyleBuilder.AlignmentPositionType is an alias for NXOpen.Annotations.TableSectionStyleBuilderAlignmentPositionType

class NXOpen.Annotations.TableSectionStyleBuilderAlignmentPositionType

Bases: object

Represents the alignment position type

Enum Members

Enum Member Enum Member Description
TopLeft
Top Left
TopRight
Top Right
BottomLeft
Bottom Left
BottomRight
Bottom right
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.