TableColumnBuilder Class

class NXOpen.Annotations.TableColumnBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Annotations.TableColumnBuilder.

This class queries and sets settings specific to parts list column when creating or editing parts list settings.

New in version NX9.0.0.

Properties

Property Description
AttributeName Returns or sets the attribute name specifies the attribute name for cells in column.
Category Returns or sets the category specifies the type of column.
DefaultText Returns or sets the default text specifies the default text set for the column cells.
IncludeNestedAssemblies Returns or sets the include nested assy specified the nested assy setting.
KeyField Returns or sets the key field specifies whether column is key column.
ProtectCells Returns or sets the protect cells specifies whether cells of column are protected.
Scope Returns or sets the scope enum specifies whether settings are to be applied to all cells of column or only cells of new rows in column.
SelectParentComponent Returns the select parent component.
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

TableColumnBuilderCategoryType Enumeration The options specify the type of column.
TableColumnBuilderScopeType Enumeration The options determine whether to apply settings to all cells or only to cells of new rows.

Property Detail

AttributeName

TableColumnBuilder.AttributeName

Returns or sets the attribute name specifies the attribute name for cells in column.

-------------------------------------

Getter Method

Signature AttributeName()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AttributeName(attributeName)

Parameters:attributeName (str) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Category

TableColumnBuilder.Category

Returns or sets the category specifies the type of column.

-------------------------------------

Getter Method

Signature Category()

Returns:
Return type:NXOpen.Annotations.TableColumnBuilderCategoryType

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Category(category)

Parameters:category (NXOpen.Annotations.TableColumnBuilderCategoryType) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

DefaultText

TableColumnBuilder.DefaultText

Returns or sets the default text specifies the default text set for the column cells.

-------------------------------------

Getter Method

Signature DefaultText()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DefaultText(defaultText)

Parameters:defaultText (str) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

IncludeNestedAssemblies

TableColumnBuilder.IncludeNestedAssemblies

Returns or sets the include nested assy specified the nested assy setting.

-------------------------------------

Getter Method

Signature IncludeNestedAssemblies()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature IncludeNestedAssemblies(includeNestedAssemblies)

Parameters:includeNestedAssemblies (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

KeyField

TableColumnBuilder.KeyField

Returns or sets the key field specifies whether column is key column.

-------------------------------------

Getter Method

Signature KeyField()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature KeyField(keyField)

Parameters:keyField (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ProtectCells

TableColumnBuilder.ProtectCells

Returns or sets the protect cells specifies whether cells of column are protected.

-------------------------------------

Getter Method

Signature ProtectCells()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ProtectCells(protectCells)

Parameters:protectCells (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Scope

TableColumnBuilder.Scope

Returns or sets the scope enum specifies whether settings are to be applied to all cells of column or only cells of new rows in column.

-------------------------------------

Getter Method

Signature Scope()

Returns:
Return type:NXOpen.Annotations.TableColumnBuilderScopeType

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Scope(scope)

Parameters:scope (NXOpen.Annotations.TableColumnBuilderScopeType) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

SelectParentComponent

TableColumnBuilder.SelectParentComponent

Returns the select parent component.

-------------------------------------

Getter Method

Signature SelectParentComponent()

Returns:
Return type:NXOpen.SelectDisplayableObject

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

TableColumnBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.