SymmetricalCenterlineBuilderTypes Enumeration¶
NXOpen.Annotations.SymmetricalCenterlineBuilder.Types is an alias for NXOpen.Annotations.SymmetricalCenterlineBuilderTypes
-
class
NXOpen.Annotations.
SymmetricalCenterlineBuilderTypes
¶ Bases:
object
the valid types of Symmetrical Centerline
Enum Members
Enum Member Enum Member Description FromFace Centerline from faceStartAndEnd Centerline from start and end point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-