SymbolWorkflowBuilder Class

class NXOpen.Annotations.SymbolWorkflowBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Annotations.SymbolWorkflowBuilder

New in version NX9.0.0.

Properties

Property Description
SymbolAutoUpdate Returns or sets the symbol auto update determines whether or not unlocked, associative custom symbol instances update automatically
SymbolSmashToSketch Returns or sets the symbol smash to sketch specifies if curve objects in symbols are added to a sketch on custom symbol smash
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

SymbolAutoUpdate

SymbolWorkflowBuilder.SymbolAutoUpdate

Returns or sets the symbol auto update determines whether or not unlocked, associative custom symbol instances update automatically

-------------------------------------

Getter Method

Signature SymbolAutoUpdate()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SymbolAutoUpdate(symbolAutoUpdate)

Parameters:symbolAutoUpdate (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

SymbolSmashToSketch

SymbolWorkflowBuilder.SymbolSmashToSketch

Returns or sets the symbol smash to sketch specifies if curve objects in symbols are added to a sketch on custom symbol smash

-------------------------------------

Getter Method

Signature SymbolSmashToSketch()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SymbolSmashToSketch(symbolSmashToSketch)

Parameters:symbolSmashToSketch (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

Validate

SymbolWorkflowBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.