Symbol Enumeration¶
-
class
NXOpen.Annotations.
Symbol
¶ Bases:
object
Specifies the elementary weld symbol Enum Members
- (ISO and DIN only, only on one side of reference line) “
- “Stud”, ” Specifies stud weld symbol (Arrow side only ) ” “Surfacing”, ” Specifies surfacing weld symbol (ISO and DIN only) ” “Intermittent”, ” Specifies intermittent weld symbol (ESKD only) ” “BackingPlate”, ” Specifies backing plate weld symbol (GB only) ” “NotSpecified”, ” Specifies weld symbol not specified ” “Last”, ” Last enum value. Should not be used. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.