SurfaceFinishBuilderStandardType Enumeration

NXOpen.Annotations.SurfaceFinishBuilder.StandardType is an alias for NXOpen.Annotations.SurfaceFinishBuilderStandardType

class NXOpen.Annotations.SurfaceFinishBuilderStandardType

Bases: object

the valid types for pmi surface finish standards

Enum Members

Enum Member Enum Member Description
Ansi
ANSI
Iso
ISO
Jis
JIS
Din
DIN
Iso2002
ISO 2002
Din2002
DIN 2002
Gb
GB131-93
Eskd
ESKD
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.