SurfaceFinishBuilderFinishType Enumeration

NXOpen.Annotations.SurfaceFinishBuilder.FinishType is an alias for NXOpen.Annotations.SurfaceFinishBuilderFinishType

class NXOpen.Annotations.SurfaceFinishBuilderFinishType

Bases: object

the valid types for pmi finish type

Enum Members

Enum Member Enum Member Description
Basic
Basic
Modifier
Modifier
ModifierAllAround
Modifier, All Around
MaterialRemovalRequired
Material Removal Required
ModifierMaterialRemovalRequired
Modifier, Material Removal Required
ModifierMaterialRemovalRequiredAllAround
Modifier, Material Removal Required, All Around
MaterialRemovalProhibited
Material Removal Prohibited
ModifierMaterialRemovalProhibited
Modifier, Material Removal Prohibited
ModifierMaterialRemovalProhibitedAllAround
Modifier, Material Removal Prohibited, All Around
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.