ShipDraftingFramebarGeneralBuilder Class¶
-
class
NXOpen.Annotations.
ShipDraftingFramebarGeneralBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.ShipDraftingFramebarGeneralBuilder
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
DecimalPlaces | Returns or sets the decimal places |
Tag | Returns the Tag for this object. |
TicDirection | Returns or sets the tic direction |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShipDraftingFramebarGeneralBuilderTicDirectionTypes Enumeration | Tic Direction Options |
Property Detail¶
DecimalPlaces¶
-
ShipDraftingFramebarGeneralBuilder.
DecimalPlaces
¶ Returns or sets the decimal places
-------------------------------------
Getter Method
Signature
DecimalPlaces()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DecimalPlaces(decimalPlaces)
Parameters: decimalPlaces (int) – New in version NX9.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
TicDirection¶
-
ShipDraftingFramebarGeneralBuilder.
TicDirection
¶ Returns or sets the tic direction
-------------------------------------
Getter Method
Signature
TicDirection()
Returns: Return type: NXOpen.Annotations.ShipDraftingFramebarGeneralBuilderTicDirectionTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TicDirection(ticDirection)
Parameters: ticDirection ( NXOpen.Annotations.ShipDraftingFramebarGeneralBuilderTicDirectionTypes
) –New in version NX9.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
Method Detail¶
Validate¶
-
ShipDraftingFramebarGeneralBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.