SearchModelViewBuilderPmiTypes Enumeration

NXOpen.Annotations.SearchModelViewBuilder.PmiTypes is an alias for NXOpen.Annotations.SearchModelViewBuilderPmiTypes

class NXOpen.Annotations.SearchModelViewBuilderPmiTypes

Bases: object

the search criteria pmitype

Enum Members

Enum Member Enum Member Description
Dimension
dimension type
FeatureControlFrame
feature control frame type
DatumFeatureSymbol
datum feature symbol type
DatumTarget
datum target type
SurfaceFinish
surface finish type
Note
note type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.