SearchCriteriaSurfaceFinishBuilderToleranceTypeOptions Enumeration

NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilder.ToleranceTypeOptions is an alias for NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilderToleranceTypeOptions

class NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilderToleranceTypeOptions

Bases: object

Lists the Tolerance type of surface finish value

Enum Members

Enum Member Enum Member Description
NoTolerance
no tolerance
EqualBilateral
equal bilateral
Bilateral
bilateral
UnilateralPlus
unilateral +
UnilateralMinus
unilateral -
PlusLimit2Lines
  • limit 2 lines
MinusLimit2Lines
  • limit 2 lines
PlusLimit1Line
  • limit 1 line
NegposlimitMinusLimit1Line
negposlimit- limit 1 line
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.