SearchCriteriaSurfaceFinishBuilderSurfaceFinishTypes Enumeration

NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilder.SurfaceFinishTypes is an alias for NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilderSurfaceFinishTypes

class NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilderSurfaceFinishTypes

Bases: object

Lists the search pmi surface finish type

Enum Members

Enum Member Enum Member Description
Open
open
OpenAndModifier
open and modifier
OpenAndModifierAndAllAround
opem and modifier and all around
Required
required
RequiredAndModifier
required and modifier
RequiredAndModifierAndAllAround
required and modifier and all around
Prohibited
prohibited
ProhibitedAndModifier
prohibiter and modifier
ProhibitedAndModifierAndAllAround
prohibiter and modifier and all around
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.