SearchCriteriaDimensionBuilderToleranceTypes Enumeration¶
NXOpen.Annotations.SearchCriteriaDimensionBuilder.ToleranceTypes is an alias for NXOpen.Annotations.SearchCriteriaDimensionBuilderToleranceTypes
-
class
NXOpen.Annotations.
SearchCriteriaDimensionBuilderToleranceTypes
¶ Bases:
object
Specifies tolerance types
Enum Members
Enum Member Enum Member Description NoTolerance NoToleranceEqualBilateralTolerance qualBilateralToleranceBilateralTolerance BilateralToleranceUnilateralPlus UnilateralPlusUnilateralMinus UnilateralMinusPlusLimitTwoLines PlusLimitTwoLinesMinusLimitTwoLines MinusLimitTwoLinesPlusLimitOneLine PlusLimitOneLineMinusLimitOneLine MinusLimitOneLineLimitsAndFits LimitsAndFitsBasic BasicReference ReferenceDiameterReference DiameterReferenceNotToScale NotToScaleBasicDimensionNotToScale BasicDimensionNotToScale-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-