SearchCriteriaDatumTargetBuilderDatumTargetTypes Enumeration

NXOpen.Annotations.SearchCriteriaDatumTargetBuilder.DatumTargetTypes is an alias for NXOpen.Annotations.SearchCriteriaDatumTargetBuilderDatumTargetTypes

class NXOpen.Annotations.SearchCriteriaDatumTargetBuilderDatumTargetTypes

Bases: object

Lists the search pmi datum target type

Enum Members

Enum Member Enum Member Description
Point
point type
Line
line type
Rectangular
rectangular type
Circular
circular type
Annular
annular type
Spherical
spherical type
Cylindrical
cylindrical type
Arbitrary
arbitray type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.