SearchCriteriaDatumTargetBuilderDatumTargetMovableOptions Enumeration

NXOpen.Annotations.SearchCriteriaDatumTargetBuilder.DatumTargetMovableOptions is an alias for NXOpen.Annotations.SearchCriteriaDatumTargetBuilderDatumTargetMovableOptions

class NXOpen.Annotations.SearchCriteriaDatumTargetBuilderDatumTargetMovableOptions

Bases: object

Represents the search pmi movable datum target type

Enum Members

Enum Member Enum Member Description
No
Datum Target
Yes
Movable Datum Target
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.