QueryPmiBuilder Class¶
-
class
NXOpen.Annotations.
QueryPmiBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.QueryPmiBuilder
To create a new instance of this class, use
NXOpen.Annotations.AnnotationManager.CreateQueryPmiBuilder()
Default values.
Property Value CreateQueryResultsView true New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AreAllOccurrencesIncluded | Returns or sets an all occurrences of selected component to be included toggle |
AreAttachedPmiIncluded | Returns or sets an attached pmi to selected geometry to be included toggle |
AreReferencingMemberObjectsIncluded | Returns or sets a referencing member objects of selected geometry to be included toggle |
CreateQueryResultsView | Returns or sets the create query results view |
Geometry | Returns the geometry |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AreAllOccurrencesIncluded¶
-
QueryPmiBuilder.
AreAllOccurrencesIncluded
¶ Returns or sets an all occurrences of selected component to be included toggle
-------------------------------------
Getter Method
Signature
AreAllOccurrencesIncluded()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
AreAllOccurrencesIncluded(areOccurrencesIncluded)
Parameters: areOccurrencesIncluded (bool) – New in version NX8.5.1.
License requirements: None.
AreAttachedPmiIncluded¶
-
QueryPmiBuilder.
AreAttachedPmiIncluded
¶ Returns or sets an attached pmi to selected geometry to be included toggle
-------------------------------------
Getter Method
Signature
AreAttachedPmiIncluded()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
AreAttachedPmiIncluded(areAttachedPMIIncluded)
Parameters: areAttachedPMIIncluded (bool) – New in version NX8.5.1.
License requirements: None.
AreReferencingMemberObjectsIncluded¶
-
QueryPmiBuilder.
AreReferencingMemberObjectsIncluded
¶ Returns or sets a referencing member objects of selected geometry to be included toggle
-------------------------------------
Getter Method
Signature
AreReferencingMemberObjectsIncluded()
Returns: Return type: bool New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
AreReferencingMemberObjectsIncluded(areReferencingMemberObjectsIncluded)
Parameters: areReferencingMemberObjectsIncluded (bool) – New in version NX8.5.1.
License requirements: None.
CreateQueryResultsView¶
-
QueryPmiBuilder.
CreateQueryResultsView
¶ Returns or sets the create query results view
-------------------------------------
Getter Method
Signature
CreateQueryResultsView()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateQueryResultsView(createQueryResultsView)
Parameters: createQueryResultsView (bool) – New in version NX8.5.0.
License requirements: None.
Geometry¶
-
QueryPmiBuilder.
Geometry
¶ Returns the geometry
-------------------------------------
Getter Method
Signature
Geometry()
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
QueryPmiBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.