PmiWaveLinkBuilder Class¶
-
class
NXOpen.Annotations.
PmiWaveLinkBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.Pmi
builderTo create a new instance of this class, use
NXOpen.Annotations.PmiWaveCollection.CreatePmiWaveLinkBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
GeometryTypeToWAVELink | Returns or sets the associated geometry type to WAVE link |
SelectedPMI | Returns the list of selected PMI to be WAVE linked |
SourcePart | Returns or sets the source part for the WAVE link |
Tag | Returns the Tag for this object. |
TargetPart | Returns or sets the target part for the WAVE link |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
GeometryTypeToWAVELink¶
-
PmiWaveLinkBuilder.
GeometryTypeToWAVELink
¶ Returns or sets the associated geometry type to WAVE link
-------------------------------------
Getter Method
Signature
GeometryTypeToWAVELink()
Returns: Return type: int New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
GeometryTypeToWAVELink(geometryType)
Parameters: geometryType (int) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SelectedPMI¶
-
PmiWaveLinkBuilder.
SelectedPMI
¶ Returns the list of selected PMI to be WAVE linked
-------------------------------------
Getter Method
Signature
SelectedPMI()
Returns: Return type: NXOpen.Annotations.SelectAnnotationList
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SourcePart¶
-
PmiWaveLinkBuilder.
SourcePart
¶ Returns or sets the source part for the WAVE link
-------------------------------------
Getter Method
Signature
SourcePart()
Returns: Return type: NXOpen.TaggedObject
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
SourcePart(sourcePart)
Parameters: sourcePart ( NXOpen.TaggedObject
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TargetPart¶
-
PmiWaveLinkBuilder.
TargetPart
¶ Returns or sets the target part for the WAVE link
-------------------------------------
Getter Method
Signature
TargetPart()
Returns: Return type: NXOpen.TaggedObject
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
TargetPart(targetPart)
Parameters: targetPart ( NXOpen.TaggedObject
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
PmiWaveLinkBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.