PmiTrackingPropertiesBuilder Class¶
-
class
NXOpen.Annotations.
PmiTrackingPropertiesBuilder
¶ Bases:
NXOpen.Builder
Represents a
Annotations.AngularDimension
builderTo create a new instance of this class, use
NXOpen.Annotations.AnnotationManager.CreatePmiTrackingPropertiesBuilder()
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetPmiTrackingPropertyStatus | Get the modified tracking status of Inherit PMI properties @return |
LoadDefaultSettings | It load default settings for all properties as defined in inherit. |
SetPmiTrackingPropertyStatus | Set the modified tracking status of Inherit PMI properties |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateTrackingProperties | Updates the Inherit PMI properties tracking list |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetPmiTrackingPropertyStatus¶
-
PmiTrackingPropertiesBuilder.
GetPmiTrackingPropertyStatus
¶ Get the modified tracking status of Inherit PMI properties
Signature
GetPmiTrackingPropertyStatus(propertyName)
Parameters: propertyName (str) – Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
LoadDefaultSettings¶
-
PmiTrackingPropertiesBuilder.
LoadDefaultSettings
¶ It load default settings for all properties as defined in inherit.
xml file
Signature
LoadDefaultSettings()
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
SetPmiTrackingPropertyStatus¶
-
PmiTrackingPropertiesBuilder.
SetPmiTrackingPropertyStatus
¶ Set the modified tracking status of Inherit PMI properties
Signature
SetPmiTrackingPropertyStatus(propertyName, propertyStatus)
Parameters: - propertyName (str) –
- propertyStatus (bool) –
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
UpdateTrackingProperties¶
-
PmiTrackingPropertiesBuilder.
UpdateTrackingProperties
¶ Updates the Inherit PMI properties tracking list
Signature
UpdateTrackingProperties()
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
PmiTrackingPropertiesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.