PmiFilterFilterType Enumeration

NXOpen.Annotations.PmiFilter.FilterType is an alias for NXOpen.Annotations.PmiFilterFilterType

class NXOpen.Annotations.PmiFilterFilterType

Bases: object

Represents a type of PMI filter that can be created using the Part Navigator.

Enum Members

Enum Member Enum Member Description
ByType
Specifies a PMI filter defined by a set of PMI types
ByView
Specifies a PMI filter defined by a set of component model views
ByComponent
Specifies a PMI filter defined by a set of components
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.