PmiFilterByTypeType Enumeration¶
NXOpen.Annotations.PmiFilterByType.Type is an alias for NXOpen.Annotations.PmiFilterByTypeType
-
class
NXOpen.Annotations.
PmiFilterByTypeType
¶ Bases:
object
Represents a PMI type that is assigned to the PMI filter.
Enum Members
Enum Member Enum Member Description Dimension Indicates a PMI dimension typeFeatureControlFrame Indicates a PMI feature control frame typeDatum Indicates a PMI datum feature typeDatumTarget Indicates a PMI datum target typeNote Indicates a PMI note typeGeneralNote Indicates a PMI general note typeSpecificNote Indicates a PMI specific note typeCoordinateNote Indicates a PMI coordinate note typeBalloonNote Indicates a PMI balloon typeCustomSymbol Indicates a PMI custom symbol typeCenterline Indicates a PMI centerline typeLineWeld Indicates a PMI weld typeCrosshatch Indicates a PMI crosshatch typeMaterial Indicates a PMI material typeSurfaceFinish Indicates a PMI surface finish typeLocator Indicates a PMI locator typeEnterpriseIdentifier Indicates a PMI enterprise identifier typeProcess Indicates a PMI process typePartIdentifier Indicates a PMI part identifier typeEmarking Indicates a PMI e-Marking typeUrl Indicates a PMI URL typeUserDefined Indicates a PMI user defined typeGeometry Indicates a PMI Geometry typeCuttingPlaneSymbol Indicates a PMI Cutting Symbol Type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-