PmiData Class¶
-
class
NXOpen.Annotations.
PmiData
¶ Bases:
NXOpen.TransientObject
Represents PMI(Product and Manufacturing Information) data
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetAssociatedObject | Returns the associated object @return Associated objects |
GetBusinessModifiers | Returns the business modifiers @return List of business modifiers |
GetIndex | Returns the index @return |
GetNumAssociatedObjectsSets | Returns the numbers of associated objects list @return |
SetAssociatedObject | Sets the associated object |
SetBusinessModifiers | Sets the business modifiers |
SetIndex | Sets the index |
SetNumAssociatedObjectsSets | Sets the number of associated objects list |
Method Detail¶
Dispose¶
-
PmiData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetAssociatedObject¶
-
PmiData.
GetAssociatedObject
¶ Returns the associated object
Signature
GetAssociatedObject()
Returns: Associated objects Return type: NXOpen.Annotations.AssociatedObject
New in version NX4.0.0.
License requirements: None.
GetBusinessModifiers¶
-
PmiData.
GetBusinessModifiers
¶ Returns the business modifiers
Signature
GetBusinessModifiers()
Returns: List of business modifiers Return type: list of NXOpen.Annotations.BusinessModifier
New in version NX4.0.0.
License requirements: None.
GetIndex¶
-
PmiData.
GetIndex
¶ Returns the index
Signature
GetIndex()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
GetNumAssociatedObjectsSets¶
-
PmiData.
GetNumAssociatedObjectsSets
¶ Returns the numbers of associated objects list
Signature
GetNumAssociatedObjectsSets()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
SetAssociatedObject¶
-
PmiData.
SetAssociatedObject
¶ Sets the associated object
Signature
SetAssociatedObject(assocObj)
Parameters: assocObj ( NXOpen.Annotations.AssociatedObject
) – List of new associated objectsNew in version NX4.0.0.
License requirements: None.
SetBusinessModifiers¶
-
PmiData.
SetBusinessModifiers
¶ Sets the business modifiers
Signature
SetBusinessModifiers(businessModifiers)
Parameters: businessModifiers (list of NXOpen.Annotations.BusinessModifier
) – List of new business modifiersNew in version NX4.0.0.
License requirements: None.
SetIndex¶
-
PmiData.
SetIndex
¶ Sets the index
Signature
SetIndex(index)
Parameters: index (int) – New in version NX5.0.0.
License requirements: None.
SetNumAssociatedObjectsSets¶
-
PmiData.
SetNumAssociatedObjectsSets
¶ Sets the number of associated objects list
Signature
SetNumAssociatedObjectsSets(numAssocObjectsSets)
Parameters: numAssocObjectsSets (int) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)