PlaneBuilderPlaneMethodType Enumeration

NXOpen.Annotations.PlaneBuilder.PlaneMethodType is an alias for NXOpen.Annotations.PlaneBuilderPlaneMethodType

class NXOpen.Annotations.PlaneBuilderPlaneMethodType

Bases: object

method used to compute the annotation plane

Enum Members

Enum Member Enum Member Description
XyPlane
XY of the WCS
XzPlane
XZ of the WCS
YzPlane
YZ of the WCS
ModelView
Model view plane
UserDefined
User define plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.