PartsListBuilder Class

class NXOpen.Annotations.PartsListBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Annotations.PartsListBuilder.

This class queries and sets settings specific to parts list when creating or editing parts list settings.

This is a sub-builder class and cannot be directly instantiated

New in version NX9.0.0.

Properties

Property Description
AllowManualRows Returns or sets the allow manual rows option that determines whether or not manual rows are allowed to be inserted into a parts list
AutomaticUpdate Returns or sets the automatic update option to determine whether or not the parts list updates automatically whenever a change occurs to a referenced object in the model
CalloutSuffix Returns or sets the callout suffix specifies the suffix to be used for reference symbol text
CharToSkip Returns or sets the characters to skip specifies the characters to be skipped for callouts
CreateNewRowAsLocked Returns or sets the create new row as locked option that determines whether new rows in the parts list are locked automatically on creation
GrowDirectionOptions Returns or sets the grow direction options that specify the direction of growth for the parts list
HighlightColor Returns or sets the highlight color specifies the color used for the delimiters that highlight manual cell text
HighlightManualText Returns or sets the highlight manual text specifies whether manual cell text is to be highlighted by delimiters
Increment Returns or sets the increment specifies the value by which consecutive callout values are be incremented
InitialCallout Returns or sets the initial callout specifies the text string used to represent the first callout in the parts list
LockPartsListSetup Returns or sets the Lock Parts List Setup option that determines Is the parts list setup protected/locked
MainSymbolCustomText Returns or sets the main symbol custom text specifies the custom text to display in the main callout symbol
MainSymbolText Returns or sets the main symbol text specifies the text to display in the main callout symbol
ReferenceSymbolCustomText Returns or sets the reference symbol custom text specifies the custom text to display in the main callout symbol
ReferenceSymbolText Returns or sets the reference symbol text specifies the text to display in the reference callout symbol
ShowLockedDeletedRows Returns or sets the show locked deleted rows option to show rows that are locked, but reference components that have been removed from the assembly
ShowReferenceCalloutSuffix Returns or sets the flag indicating whether the reference callout suffix will be displayed.
SortOnUpdate Returns or sets the sort on update option that determines whether or not the parts list sorts automatically during update
Symbol Returns or sets the symbol type specifies the balloon type used to call out members
Tag Returns the Tag for this object.
VerticalGroupAttachment Returns or sets the leader attachment to vertical callout groups

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

PartsListBuilderPartsListGrowDirectionOptions Enumeration Grow direction options The options specify the direction of growth for the parts list
PartsListBuilderPartsListMainSymbolText Enumeration Main Symbol Text Types Specifies the text to display in the main callout symbol
PartsListBuilderPartsListReferenceSymbolText Enumeration Reference Symbol Text Types Specifies the text to display in the reference callout symbol
PartsListBuilderPartsListShowLockedDeletedRows Enumeration Locked deleted rows options The options specify how to show rows that are locked, but reference components that have been removed from the assembly
PartsListBuilderPartsListSymbolType Enumeration Symbol Types The types specify the balloon type used to call out members
PartsListBuilderPartsListVerticalGroupLeaderAttachment Enumeration Represents leader attachment for vertical callout groups.

Property Detail

AllowManualRows

PartsListBuilder.AllowManualRows

Returns or sets the allow manual rows option that determines whether or not manual rows are allowed to be inserted into a parts list

-------------------------------------

Getter Method

Signature AllowManualRows()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AllowManualRows(allowManualRows)

Parameters:allowManualRows (bool) –

New in version NX9.0.0.

License requirements: None.

AutomaticUpdate

PartsListBuilder.AutomaticUpdate

Returns or sets the automatic update option to determine whether or not the parts list updates automatically whenever a change occurs to a referenced object in the model

-------------------------------------

Getter Method

Signature AutomaticUpdate()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AutomaticUpdate(automaticUpdate)

Parameters:automaticUpdate (bool) –

New in version NX9.0.0.

License requirements: None.

CalloutSuffix

PartsListBuilder.CalloutSuffix

Returns or sets the callout suffix specifies the suffix to be used for reference symbol text

-------------------------------------

Getter Method

Signature CalloutSuffix()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CalloutSuffix(calloutSuffix)

Parameters:calloutSuffix (str) –

New in version NX9.0.0.

License requirements: None.

CharToSkip

PartsListBuilder.CharToSkip

Returns or sets the characters to skip specifies the characters to be skipped for callouts

-------------------------------------

Getter Method

Signature CharToSkip()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CharToSkip(charsToSkip)

Parameters:charsToSkip (str) –

New in version NX9.0.0.

License requirements: None.

CreateNewRowAsLocked

PartsListBuilder.CreateNewRowAsLocked

Returns or sets the create new row as locked option that determines whether new rows in the parts list are locked automatically on creation

-------------------------------------

Getter Method

Signature CreateNewRowAsLocked()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreateNewRowAsLocked(createNewRowAsLocked)

Parameters:createNewRowAsLocked (bool) –

New in version NX9.0.0.

License requirements: None.

GrowDirectionOptions

PartsListBuilder.GrowDirectionOptions

Returns or sets the grow direction options that specify the direction of growth for the parts list

-------------------------------------

Getter Method

Signature GrowDirectionOptions()

Returns:
Return type:NXOpen.Annotations.PartsListBuilderPartsListGrowDirectionOptions

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature GrowDirectionOptions(growDirectionOptions)

Parameters:growDirectionOptions (NXOpen.Annotations.PartsListBuilderPartsListGrowDirectionOptions) –

New in version NX9.0.0.

License requirements: None.

HighlightColor

PartsListBuilder.HighlightColor

Returns or sets the highlight color specifies the color used for the delimiters that highlight manual cell text

-------------------------------------

Getter Method

Signature HighlightColor()

Returns:
Return type:Id

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature HighlightColor(highlightColor)

Parameters:highlightColor (Id) –

New in version NX9.0.0.

License requirements: None.

HighlightManualText

PartsListBuilder.HighlightManualText

Returns or sets the highlight manual text specifies whether manual cell text is to be highlighted by delimiters

-------------------------------------

Getter Method

Signature HighlightManualText()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature HighlightManualText(highlightManualText)

Parameters:highlightManualText (bool) –

New in version NX9.0.0.

License requirements: None.

Increment

PartsListBuilder.Increment

Returns or sets the increment specifies the value by which consecutive callout values are be incremented

-------------------------------------

Getter Method

Signature Increment()

Returns:
Return type:int

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Increment(increment)

Parameters:increment (int) –

New in version NX9.0.0.

License requirements: None.

InitialCallout

PartsListBuilder.InitialCallout

Returns or sets the initial callout specifies the text string used to represent the first callout in the parts list

-------------------------------------

Getter Method

Signature InitialCallout()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature InitialCallout(initialCallout)

Parameters:initialCallout (str) –

New in version NX9.0.0.

License requirements: None.

LockPartsListSetup

PartsListBuilder.LockPartsListSetup

Returns or sets the Lock Parts List Setup option that determines Is the parts list setup protected/locked

-------------------------------------

Getter Method

Signature LockPartsListSetup()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LockPartsListSetup(lockPartsListSetup)

Parameters:lockPartsListSetup (bool) –

New in version NX9.0.0.

License requirements: None.

MainSymbolCustomText

PartsListBuilder.MainSymbolCustomText

Returns or sets the main symbol custom text specifies the custom text to display in the main callout symbol

-------------------------------------

Getter Method

Signature MainSymbolCustomText()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MainSymbolCustomText(mainSymbolCustomText)

Parameters:mainSymbolCustomText (str) –

New in version NX9.0.0.

License requirements: None.

MainSymbolText

PartsListBuilder.MainSymbolText

Returns or sets the main symbol text specifies the text to display in the main callout symbol

-------------------------------------

Getter Method

Signature MainSymbolText()

Returns:
Return type:NXOpen.Annotations.PartsListBuilderPartsListMainSymbolText

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MainSymbolText(mainSymbolText)

Parameters:mainSymbolText (NXOpen.Annotations.PartsListBuilderPartsListMainSymbolText) –

New in version NX9.0.0.

License requirements: None.

ReferenceSymbolCustomText

PartsListBuilder.ReferenceSymbolCustomText

Returns or sets the reference symbol custom text specifies the custom text to display in the main callout symbol

-------------------------------------

Getter Method

Signature ReferenceSymbolCustomText()

Returns:
Return type:str

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ReferenceSymbolCustomText(referenceSymbolCustomText)

Parameters:referenceSymbolCustomText (str) –

New in version NX9.0.0.

License requirements: None.

ReferenceSymbolText

PartsListBuilder.ReferenceSymbolText

Returns or sets the reference symbol text specifies the text to display in the reference callout symbol

-------------------------------------

Getter Method

Signature ReferenceSymbolText()

Returns:
Return type:NXOpen.Annotations.PartsListBuilderPartsListReferenceSymbolText

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ReferenceSymbolText(referenceSymbolText)

Parameters:referenceSymbolText (NXOpen.Annotations.PartsListBuilderPartsListReferenceSymbolText) –

New in version NX9.0.0.

License requirements: None.

ShowLockedDeletedRows

PartsListBuilder.ShowLockedDeletedRows

Returns or sets the show locked deleted rows option to show rows that are locked, but reference components that have been removed from the assembly

-------------------------------------

Getter Method

Signature ShowLockedDeletedRows()

Returns:
Return type:NXOpen.Annotations.PartsListBuilderPartsListShowLockedDeletedRows

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ShowLockedDeletedRows(showLockedDeletedRows)

Parameters:showLockedDeletedRows (NXOpen.Annotations.PartsListBuilderPartsListShowLockedDeletedRows) –

New in version NX9.0.0.

License requirements: None.

ShowReferenceCalloutSuffix

PartsListBuilder.ShowReferenceCalloutSuffix

Returns or sets the flag indicating whether the reference callout suffix will be displayed.

A value of true indicates that the suffix will be displayed.

-------------------------------------

Getter Method

Signature ShowReferenceCalloutSuffix()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ShowReferenceCalloutSuffix(showReferenceCalloutSuffix)

Parameters:showReferenceCalloutSuffix (bool) –

New in version NX9.0.0.

License requirements: None.

SortOnUpdate

PartsListBuilder.SortOnUpdate

Returns or sets the sort on update option that determines whether or not the parts list sorts automatically during update

-------------------------------------

Getter Method

Signature SortOnUpdate()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SortOnUpdate(sortOnUpdate)

Parameters:sortOnUpdate (bool) –

New in version NX9.0.0.

License requirements: None.

Symbol

PartsListBuilder.Symbol

Returns or sets the symbol type specifies the balloon type used to call out members

-------------------------------------

Getter Method

Signature Symbol()

Returns:
Return type:NXOpen.Annotations.PartsListBuilderPartsListSymbolType

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Symbol(symbol)

Parameters:symbol (NXOpen.Annotations.PartsListBuilderPartsListSymbolType) –

New in version NX9.0.0.

License requirements: None.

VerticalGroupAttachment

PartsListBuilder.VerticalGroupAttachment

Returns or sets the leader attachment to vertical callout groups

-------------------------------------

Getter Method

Signature VerticalGroupAttachment()

Returns:
Return type:NXOpen.Annotations.PartsListBuilderPartsListVerticalGroupLeaderAttachment

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature VerticalGroupAttachment(position)

Parameters:position (NXOpen.Annotations.PartsListBuilderPartsListVerticalGroupLeaderAttachment) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

Validate

PartsListBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.