OrdinatePositiveDirection Enumeration

class NXOpen.Annotations.OrdinatePositiveDirection

Bases: object

Specifies the positive direction for ordinate dimensions Enum Members

Enum Member Enum Member Description
All
Specifies positive direction for all dimensions
UpperRight
Specifies positive direction for dimensions in upper right qudrant
UpperLeft
Specifies positive direction for dimensions in upper left qudrant
LowerRight
Specifies positive direction for dimensions in lower right qudrant
LowerLeft
Specifies positive direction for dimensions in lower left qudrant
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.