OrdinateOriginDisplayOption Enumeration

class NXOpen.Annotations.OrdinateOriginDisplayOption

Bases: object

Specifies the ordinate origin dimension display option Enum Members

Enum Member Enum Member Description
UserDefinedSymbol
Displays user defined symbol at the ordinate origin
OrdinateSetName
Displays the ordinate set name at the ordinate origin
NoText
Display no text at the ordinate origin
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.