OrdinateDoglegDefinition Enumeration

class NXOpen.Annotations.OrdinateDoglegDefinition

Bases: object

Specifies the ordinate dimension dogleg definition

A - Start offset

B - End offset

C - Dog leg angle

<code> _____________ Dimension Line | | B | _______ | A / / . / .C / Dogleg Segement . / _______./ | | </code>

Enum Members

Enum Member Enum Member Description
StartAndEnd
Specifies start and end offeset defined
StartAngle
Specifies start offset and dogleg angle defined
EndAngle
Specifies end offset and dogleg angle defined
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.