OrdinateDoglegCreationOption Enumeration

class NXOpen.Annotations.OrdinateDoglegCreationOption

Bases: object

Specifies the dogleg creation option when creating/editing the ordinate dimension Enum Members

Enum Member Enum Member Description
Infer
Software infers whether the dogleg would be created
Yes
Dogleg will always be created
No
Dogleg will not be created
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.