OffsetCenterPointBuilderOffset Enumeration¶
NXOpen.Annotations.OffsetCenterPointBuilder.Offset is an alias for NXOpen.Annotations.OffsetCenterPointBuilderOffset
-
class
NXOpen.Annotations.
OffsetCenterPointBuilderOffset
¶ Bases:
object
the valid offset method types
Enum Members
Enum Member Enum Member Description HorizontalDistanceFromArc horizontal distance from arcHorizontalDistanceFromCenter horizontal distance from centerHorizontalDistanceByPosition horizontal distance by position, applicable only for creationVerticalDistanceFromArc vertical distance from arcVerticalDistanceFromCenter vertical distance from centerVerticalDistanceByPosition vertical distance by position, applicable only for creation-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-