NoteData Class

class NXOpen.Annotations.NoteData

Bases: NXOpen.TransientObject

Represents note data

New in version NX4.0.0.

Methods

Method Description
Dispose Frees the object from memory.
GetSimpleDraftingAidPreferences Returns the SimpleDraftingAidPreferences object @return Note preferences
GetText Returns the text @return List of lines
SetSimpleDraftingAidPreferences Sets the SimpleDraftingAidPreferences object
SetText Sets the text

Method Detail

Dispose

NoteData.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX4.0.0.

License requirements: None.

GetSimpleDraftingAidPreferences

NoteData.GetSimpleDraftingAidPreferences

Returns the SimpleDraftingAidPreferences object

Signature GetSimpleDraftingAidPreferences()

Returns:Note preferences
Return type:NXOpen.Annotations.SimpleDraftingAidPreferences

New in version NX4.0.0.

License requirements: None.

GetText

NoteData.GetText

Returns the text

Signature GetText()

Returns:List of lines
Return type:list of str

New in version NX4.0.0.

License requirements: None.

SetSimpleDraftingAidPreferences

NoteData.SetSimpleDraftingAidPreferences

Sets the SimpleDraftingAidPreferences object

Signature SetSimpleDraftingAidPreferences(preferences)

Parameters:preferences (NXOpen.Annotations.SimpleDraftingAidPreferences) – New note preferences

New in version NX4.0.0.

License requirements: None.

SetText

NoteData.SetText

Sets the text

Signature SetText(lines)

Parameters:lines (list of str) – List of new lines

New in version NX4.0.0.

License requirements: None.