MaterialConditionModifier Enumeration

class NXOpen.Annotations.MaterialConditionModifier

Bases: object

Specifies the material condition modifier Enum Members

should be used in place of the RFS for ASME 1994 and ISO standards “

“Last”, ” Last enum value. Should not be used. “
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.