LineWidth Enumeration¶
-
class
NXOpen.Annotations.
LineWidth
¶ Bases:
object
Specifies the line width.
When using a standard font in the
NXOpen.Annotations.LetteringStyleBuilder
the values forNXOpen.Annotations.LineWidth
will be interpreted as follows: A value ofNXOpen.Annotations.LineWidth.Thin
is equivalent to a font style value of “Regular” or “Italic” (if italic is set). Any value other thanNXOpen.Annotations.LineWidth.Thin
is equivalent to a font style value of “Bold” or “Bold Italic” (if italic is set). This applies to:NXOpen.Annotations.LetteringStyleBuilder.DimensionTextLineWidth`()
with respect toNXOpen.Annotations.LetteringStyleBuilder.DimensionTextItalicized`()
NXOpen.Annotations.LetteringStyleBuilder.AppendedTextLineWidth`()
with respect toNXOpen.Annotations.LetteringStyleBuilder.AppendedTextItalicized`()
NXOpen.Annotations.LetteringStyleBuilder.ToleranceTextLineWidth`()
with respect toNXOpen.Annotations.LetteringStyleBuilder.ToleranceTextItalicized`()
NXOpen.Annotations.LetteringStyleBuilder.GeneralTextLineWidth`()
with respect toNXOpen.Annotations.LetteringStyleBuilder.GeneralTextItalicized`()
Enum MembersEnum Member Enum Member Description Normal Thick Thin One Width OneTwo Width TwoThree Width ThreeFour Width FourFive Width FiveSix Width SixSeven Width SevenEight Width EightNine Width Nine-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-