LineComponentLineType Enumeration

NXOpen.Annotations.LineComponent.LineType is an alias for NXOpen.Annotations.LineComponentLineType

class NXOpen.Annotations.LineComponentLineType

Bases: object

the line type

Enum Members

Enum Member Enum Member Description
Extension
extension line
Leader
leader line
NarrowLeader
narrow leader line
Stub
stub line
DualBracket
dual bracket
Annotation
annotation line
Inspection
inspection line
SecondaryExtension
secondary extension
Tolerance
tolerance line
Jog
jog line
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.