LightweightSectionBuilder Class¶
-
class
NXOpen.Annotations.
LightweightSectionBuilder
¶ Bases:
NXOpen.Display.DynamicSectionBuilder
Represents a
NXOpen.Annotations.LightweightSection
builderTo create a new instance of this class, use
NXOpen.Annotations.PmiLightweightSectionCollection.CreateLightweightSectionBuilder()
Default values.
Property Value BoxExtentDelayUpdate false CapColorOption Any ClipType Section CurveColorOption Any CuttingPlaneSymbol.DisplayCuttingPlaneSymbol 0 CuttingPlaneSymbol.UseTwoArrows 0 CuttingPlaneSymbol.ViewNameFormat UserDefined LockPlanes true ShowCap true ShowClip true ShowCurves (deprecated) false ShowGrid false ShowInterference false ShowViewer false Type OnePlane New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AssemblyCrosshatching | Returns or sets the assembly crosshatch option |
BoundingBoxComponents | Returns the objects to define the box section type bounding extents |
BoxExtentDelayUpdate | Returns or sets the delay box extent update. |
BoxExtentMargin | Returns or sets the margin for box section extents |
BoxExtentObjects | Returns the objects that define the extents for box section. |
BoxExtentSupported | Returns the box extent support. |
CapColor | Returns or sets the cap color. |
CapColorOption | Returns or sets the cap color option |
ClipCoplanarObjects | Returns or sets the clip coplanar objects |
ClipType | Returns or sets the clip type |
CrosshatchSettings | Returns the crosshatch settings |
CsysType | Returns or sets the coordinate system used for creating section plane along X, Y or Z principal planes. |
CurveColor | Returns or sets the curve color. |
CurveColorOption | Returns or sets the curve color option |
CuttingPlaneSymbol | Returns the cutting plane symbol |
DeferCurveUpdate | Returns or sets the defer curve update property. |
DisplayCrosshatch | Returns or sets the display crosshatch option |
InterferenceColor | Returns or sets the interference color. |
LayerSettings | Returns the layer settings builder |
LockPlanes | Returns or sets the lock planes flag. |
NumberInSeries | Returns or sets the number of requested section planes in the current section series. |
ObjectsToSection | Returns the objects to section |
PatternDefinedBy | Returns or sets the crosshatch pattern defined by |
RestrictCrosshatch | Returns or sets the restrict crosshatch angle to 45 degree option |
ReverseSeries | Returns or sets the reverse series flag |
SaveAssociativeCurves | Returns or sets the save associative curves toggle value |
SeriesSpacing | Returns or sets the section plane spacing in the current section series. |
ShowCap | Returns or sets the cap on off flag |
ShowClip | Returns or sets the clip on off flag |
ShowCurves | Returns or sets the curve on off flag. |
ShowGrid | Returns or sets the show grid display flag |
ShowInterference | Returns or sets the interference on off flag. |
ShowViewer | Returns or sets the 2D viewer display flag |
Tag | Returns the Tag for this object. |
ToleranceCrosshatch | Returns or sets the crosshatch adjacency tolerance |
Type | Returns or sets the section type |
View | Returns or sets the modeling view in which section object edits are being done. |
ViewName | Returns or sets the name of the lightweight section view |
Methods¶
Method | Description |
---|---|
AlternatePlane | Cycle through planes that are 90 degrees aligned to the current section plane. |
Commit | Commits any edits that have been applied to the builder. |
CreateDatumPlane | Creates a datum plane from the active section plane. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditView | Edits the section object in the modeling view. |
GetActivePlane | Gets the active plane in the section. |
GetAllPlanesGeometry | Gets geometry for all planes of the section. |
GetBoundingBox | Gets bounding box used by the section. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetGridSettings | Creates a grid settings builder from the active section plane. |
GetName | Gets the section name. |
GetNormal | Gets the normal of the section plane @return Section plane normal |
GetObject | Returns the object currently being edited by this builder. |
GetOffset | Gets the the plane offset. |
GetOffsetLimits | Gets minimum and maximum offset limits. |
GetOrigin | Gets the section origin. |
GetPlaneGeometry | Gets geometry of specified plane of the section. |
GetPlaneThickness | Gets the thickness between active plane pair. |
GetRotationAngle | Gets rotation angle for specified axis. |
GetRotationMatrix | Gets the section rotation matrix @return Rotation matrix |
GetSectionCurves | Returns the lightweight section view curves |
IsAssociativitySupported | Determines if an associative section plane is supported. |
LoadAllIntersecting | Loads all components that intersect the current section plane. |
LoadNearIntersecting | Loads components that intersect the current section plane and are near the section plane origin. |
OffsetOriginInPlane | Offsets section origin within current section plane. |
PlaneX | Creates a plane along X direction. |
PlaneY | Creates a plane along Y direction. |
PlaneZ | Creates a plane along Z direction. |
RestoreView | Restores the section to the saved section in the view database. |
ReverseDirection | Reverses the plane direction. |
SaveCurves | Creates curves by intersecting all clipping planes of the section with all visible bodies in the scene and adds them to the group created with the specified name. |
SetActivePlane | Sets the active plane in the section |
SetAllPlanesGeometry | Sets geometry for all planes of the section. |
SetAssociativePlane | Makes dynamic section associative to the specified plane The plane must be a smart plane; otherwise an error will be reported. |
SetBoundingBox | Sets bounding box for the section. |
SetDefaultPlane | Set current section plane to its default definition. |
SetDefaults | Set current section to the default values. |
SetName | Sets the section name. |
SetNormal | Sets the normal of the section plane |
SetOffset | Sets the the plane offset. |
SetOffsetByPoint | This method offsets the active clipping plane such that the plane passes through the specified point. |
SetOrigin | Sets the section origin. |
SetPlane | Sets a section plane to be the specified plane The plane is created at the specified origin with the specified rotation matrix. |
SetPlaneThickness | Sets the thickness between active plane pair. |
SetRotationAngle | Rotates the section about specified axis by the specified angle. |
SetRotationMatrix | Sets the section rotation matrix |
ShowCurvePreview | Show/hide curve preview. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
ShowSectionCurves | Shows the section curves in the view associated with the builder. |
UpdateBoxExtents | Update box section display by recomputing the box extents if necessary. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AssemblyCrosshatching¶
-
LightweightSectionBuilder.
AssemblyCrosshatching
¶ Returns or sets the assembly crosshatch option
-------------------------------------
Getter Method
Signature
AssemblyCrosshatching()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssemblyCrosshatching(assemblyCrosshatchingOption)
Parameters: assemblyCrosshatchingOption (bool) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”)
BoundingBoxComponents¶
-
LightweightSectionBuilder.
BoundingBoxComponents
¶ Returns the objects to define the box section type bounding extents
-------------------------------------
Getter Method
Signature
BoundingBoxComponents()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX8.0.0.
License requirements: None.
ClipCoplanarObjects¶
-
LightweightSectionBuilder.
ClipCoplanarObjects
¶ Returns or sets the clip coplanar objects
-------------------------------------
Getter Method
Signature
ClipCoplanarObjects()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClipCoplanarObjects(clipCoplanarObjectsOption)
Parameters: clipCoplanarObjectsOption (bool) – New in version NX11.0.0.
License requirements: geometric_tol (“GDT”)
CrosshatchSettings¶
-
LightweightSectionBuilder.
CrosshatchSettings
¶ Returns the crosshatch settings
-------------------------------------
Getter Method
Signature
CrosshatchSettings()
Returns: Return type: NXOpen.Annotations.HatchFillSettingsBuilder
New in version NX9.0.0.
License requirements: None.
CuttingPlaneSymbol¶
-
LightweightSectionBuilder.
CuttingPlaneSymbol
¶ Returns the cutting plane symbol
-------------------------------------
Getter Method
Signature
CuttingPlaneSymbol()
Returns: Return type: NXOpen.Annotations.CuttingPlaneSymbolBuilder
New in version NX9.0.0.
License requirements: None.
DisplayCrosshatch¶
-
LightweightSectionBuilder.
DisplayCrosshatch
¶ Returns or sets the display crosshatch option
-------------------------------------
Getter Method
Signature
DisplayCrosshatch()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayCrosshatch(displayCrosshatchOption)
Parameters: displayCrosshatchOption (bool) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”)
ObjectsToSection¶
-
LightweightSectionBuilder.
ObjectsToSection
¶ Returns the objects to section
-------------------------------------
Getter Method
Signature
ObjectsToSection()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX7.5.0.
License requirements: None.
PatternDefinedBy¶
-
LightweightSectionBuilder.
PatternDefinedBy
¶ Returns or sets the crosshatch pattern defined by
-------------------------------------
Getter Method
Signature
PatternDefinedBy()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PatternDefinedBy(patternDefinedBy)
Parameters: patternDefinedBy (int) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”)
RestrictCrosshatch¶
-
LightweightSectionBuilder.
RestrictCrosshatch
¶ Returns or sets the restrict crosshatch angle to 45 degree option
-------------------------------------
Getter Method
Signature
RestrictCrosshatch()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RestrictCrosshatch(restrictCrosshatchOption)
Parameters: restrictCrosshatchOption (bool) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”)
SaveAssociativeCurves¶
-
LightweightSectionBuilder.
SaveAssociativeCurves
¶ Returns or sets the save associative curves toggle value
-------------------------------------
Getter Method
Signature
SaveAssociativeCurves()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveAssociativeCurves(saveAssociativeCurvesToggle)
Parameters: saveAssociativeCurvesToggle (bool) – New in version NX7.5.0.
License requirements: geometric_tol (“GDT”)
ToleranceCrosshatch¶
-
LightweightSectionBuilder.
ToleranceCrosshatch
¶ Returns or sets the crosshatch adjacency tolerance
-------------------------------------
Getter Method
Signature
ToleranceCrosshatch()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToleranceCrosshatch(crosshatchAdjacencyTolerance)
Parameters: crosshatchAdjacencyTolerance (float) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”)
ViewName¶
-
LightweightSectionBuilder.
ViewName
¶ Returns or sets the name of the lightweight section view
-------------------------------------
Getter Method
Signature
ViewName()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ViewName(viewName)
Parameters: viewName (str) – Section name New in version NX7.5.0.
License requirements: geometric_tol (“GDT”)
Method Detail¶
GetSectionCurves¶
-
LightweightSectionBuilder.
GetSectionCurves
¶ Returns the lightweight section view curves
Signature
GetSectionCurves()
Returns: Array of lightweight section view curves Return type: list of NXOpen.Curve
New in version NX7.5.0.
License requirements: None.
Validate¶
-
LightweightSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.