Lettering Struct¶
-
class
NXOpen.Annotations.
Lettering
¶ Bases:
object
Specifies lettering data .
Constructor: NXOpen.Annotations.Lettering()
Fields¶
Field | Description |
---|---|
Size | Height of a character |
CharacterSpaceFactor | Multiplier applied to font’s standard character spacing |
AspectRatio | Aspect ratio for a character |
LineSpaceFactor | Multiplier applied to font’s standard line spacing |
Cfw | Color, font, and width for lettering |
Italic | italicized text for standard font text |
SymbolAspectRatio | Symbol aspect ratio (this only applies to symbols when using standard fonts) This value controls the aspect ratio of text control sequences such as the diameter symbol (represented by the <O> text control sequence), the counterbore symbol (represented by the <#C> text control sequence), the degree symbol (represented by the <$s> text control sequence), the true position symbol (represented by the <&10> text control sequence), etc. |
Size¶
-
Lettering.
Size
¶ Height of a character
-------------------------------------
Field Value Type:float
CharacterSpaceFactor¶
-
Lettering.
CharacterSpaceFactor
¶ Multiplier applied to font’s standard character spacing
-------------------------------------
Field Value Type:float
AspectRatio¶
-
Lettering.
AspectRatio
¶ Aspect ratio for a character
-------------------------------------
Field Value Type:float
LineSpaceFactor¶
-
Lettering.
LineSpaceFactor
¶ Multiplier applied to font’s standard line spacing
-------------------------------------
Field Value Type:float
Cfw¶
-
Lettering.
Cfw
¶ Color, font, and width for lettering
-------------------------------------
Field Value Type:
NXOpen.Annotations.TextCfw
Italic¶
-
Lettering.
Italic
¶ italicized text for standard font text
-------------------------------------
Field Value Type:bool
SymbolAspectRatio¶
-
Lettering.
SymbolAspectRatio
¶ Symbol aspect ratio (this only applies to symbols when using standard fonts) This value controls the aspect ratio of text control sequences such as the diameter symbol (represented by the <O> text control sequence), the counterbore symbol (represented by the <#C> text control sequence), the degree symbol (represented by the <$s> text control sequence), the true position symbol (represented by the <&10> text control sequence), etc.
This value cannot be negative. The default value is zero. A zero value indicates that the aspect ratio for a character will be used for the symbol aspect ratio.
-------------------------------------
Field Value Type:float