LeaderVerticalAttachment Enumeration¶
-
class
NXOpen.Annotations.
LeaderVerticalAttachment
¶ Bases:
object
Specifies on what a leader is attached to Enum Members
Enum Member Enum Member Description Null Should not be usedTop Attach vertically to the top of the annotationCenter Attach vertically to the center of the annotationBottom Attach vertically to the bottom of the annotationLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-