LeaderSide Enumeration¶
-
class
NXOpen.Annotations.
LeaderSide
¶ Bases:
object
Specifies which side the leader will be on Enum Members
- This is only used while interacting with NX UI “
- “Last”, ” Last enum value. Should not be used. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.