LeaderDataLeaderType Enumeration¶
NXOpen.Annotations.LeaderData.LeaderType is an alias for NXOpen.Annotations.LeaderDataLeaderType
-
class
NXOpen.Annotations.
LeaderDataLeaderType
¶ Bases:
object
the set of datatypes used to define the types of leaders that can be applied to an annotation
Enum Members
Enum Member Enum Member Description Plain Plain leader styleAllAround Plain leader style with all around symbolPlainWithoutStub Plain leader style with no stubFlag Flag styleDatum Datum feature symbol styleDotTerminated Datum feature on stub of dot terminated styleExtension Id symbol extension style leaderAllOver -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-