LeaderAttachment Enumeration

class NXOpen.Annotations.LeaderAttachment

Bases: object

Specifies what a leader is attached to Enum Members

Enum Member Enum Member Description
Null
Should not be used
OnObject
Screen
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.