LeaderAlignment Enumeration

class NXOpen.Annotations.LeaderAlignment

Bases: object

Specifies the leader’s alignment.

For more information, see the Leader Text Alignment section of Drafting Help. Enum Members

Enum Member Enum Member Description
Null
Should not be used
Top
Middle
Bottom
TextBottomMax
extend leader to maximum
TextBottomMaxUnderline
extend leader to maximum, underline all lines
TextBottom
TextBottomUnderline
underline all lines
TextTopMax
extend leader to maximum
TextTopMaxUnderline
extend leader to maximum, underline all lines
TextTop
TextTopUnderline
underline all lines
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.