IntersectionSymbolBuilderThickness Enumeration

NXOpen.Annotations.IntersectionSymbolBuilder.Thickness is an alias for NXOpen.Annotations.IntersectionSymbolBuilderThickness

class NXOpen.Annotations.IntersectionSymbolBuilderThickness

Bases: object

the types of intersection symbol thickness

Enum Members

Enum Member Enum Member Description
Thin
Thin
Normal
Normal
Thick
Thick
One
Width One
Two
Width Two
Three
Width Three
Four
Width Four
Five
Width Five
Six
Width Six
Seven
Width Seven
Eight
Width Eight
Nine
Width Nine
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.