IdentificationLineLocation Enumeration

class NXOpen.Annotations.IdentificationLineLocation

Bases: object

Specifies the weld identification line location (ISO and DIN only) Enum Members

reference line “
“Bottom”, ” Specifies identification line below the
reference line “
“Last”, ” Last enum value. Should not be used. “
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.