HoleTableSettingsFormatBuilderShowColumnsType Enumeration¶
NXOpen.Annotations.HoleTableSettingsFormatBuilder.ShowColumnsType is an alias for NXOpen.Annotations.HoleTableSettingsFormatBuilderShowColumnsType
-
class
NXOpen.Annotations.
HoleTableSettingsFormatBuilderShowColumnsType
¶ Bases:
object
Represents Show Columns options
Enum Members
Enum Member Enum Member Description Xy X and YXyz X, Y and ZAll All-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-